Page top

Lead Contents

FAQ03478 of Timers FAQ

FAQ No. FAQ03478

Primary Contents


Can H5CX Digital Timers be used as a Twin Timer?


Yes, it can be used.
H5CX is set by default to be used as Timers. To use it as Twin Timers, select the twin Timers for the timers/twin timer selection.

Twin timers output mode can be set to either flicker OFF start or flicker ON start.

Applicable models: H5CX-A and H5CX-L

Note:The H5CX-B does not have a twin timer function.

Recommended Products


A Process Indicator Ideal for Discriminating and Displaying Measurements for Voltage/Current Signals


A New High-performance Controller: High Resolution, High Speed, and High Input Accuracy. Logic Operations and Preventive Maintenance Function.


Easy to Use and Easy to Read.

Other Timers FAQ