Page top

Primary Contents

Question

What is diversity?

Answer



Common malfunctions and the probability of failure in electric products can be reduced if each product uses a variety of control circuits as well as various types of devices and components. The following are examples showing the use of diversity.

Safety door with safety components that use a combination of NC and NO contacts.

Circuits using control components that are different from each other in type.

Circuits using control components that are different from each other in type.

Redundant combinations of electromechanical and electronic circuits.

The following diagram shows an example of operating a safety door using a combination of negative operation and positive operation switches.

Recommended Products

D4N

Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards

F3SJ Ver.2

The updated F3SJ is even easier to use.

OS3101

Operator Presence Detection in Work Areas with Complex Shapes.

Other Safety Limit Switches FAQ