Page top

Primary Contents

Question

What is slow action?

Answer



SPST-NC + SPST-NO Contact (Slow Action) Example

SPST-NC + SPST-NO contact slow action has a direct opening mechanism (forcibly opened contacts) defined under EN 60497-5-1. The NC contact side is the only side with a direct opening mechanism (forcibly opened contacts).
When contact welding occur, a plunger is pushed down to open the NC contacts and break the circuit.

DPST-NC Contact (Slow Action) Example

DPST-NC contact slow action has a direct opening mechanism (forcibly opened contacts) defined under EN60497-5-1. Both NC contact sides have a direct opening mechanism (forcibly opened contacts).

Recommended Products

D4N

Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards

F3SJ Ver.2

The updated F3SJ is even easier to use.

OS3101

Operator Presence Detection in Work Areas with Complex Shapes.

Other Safety Limit Switches FAQ