![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is the difference between the Safety Limit Switches and the General Limit Switches?
Answer
The Safety Limit Switches are provided with a direct drive positive opening mechanism (positive actuation structure) with which welded portions are forcibly torn even if contact welding occurs, thus stopping a dangerous process (load) without fault and performing safe operation.
On the other hand, the General Limit Switches are not provided with the above mentioned mechanism. Therefore, if contact welding occurs, it keeps conduction state, and thus it cannot reliably stop dangerous process (load) and may perform dangerous operation.
For this reason, use the Safety Limit Switches in applications for safety purposes.
Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards
The updated F3SJ is even easier to use.
Operator Presence Detection in Work Areas with Complex Shapes.