Page top

Primary Contents

Question

Can the PLC Reporter 32 be connected to the peripheral port of a Programmable Controller?

Answer



PLC Reporter 32 supports communications in Host Link mode. The peripheral port is typically used for connection with a Programmable Controller or the CX-Programmer FA Integrated Tool Package in peripheral bus (toolbus) mode, but it can be used in Host Link mode. (Some of the old models do not support the Host Link mode.)

Settings vary with the Programmable Controller, so refer to the corresponding Programmable Controller manual.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other IT Products and Software Components FAQ