![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Is there a command that can write 100 words of data at once from a computer to the DM Area in the CPU Unit?
Answer
Yes, a FINS (Factory Interface Network Service) command is supported for CS1-series and CVM1/CV-series Programmable Controllers. This command is used to write 100 words of data all at one time. However, only the CS1-series and CVM1/CV-series support this command. When using C-series Programmable Controllers, the data must be written 4 times, writing 30 words each time. Therefore 100 words of data cannot be written simultaneously when using C-Series.
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.