Page top

Primary Contents

Question

What part of I/O memory in the CPU Unit is allocated to CS1W-SCU21 Serial Communications Unit and CS1W-CLK21 Controller Link Unit?

Answer



CS1W-SCU21 and CS1W-CLK21 are both CPU Bus Units. Words are allocated to CPU Bus Units according to the unit numbers set on the front of the Units. The first Word that is allocated is “n” and corresponds to CIO 1500 + 25 x unit number. For setting details, refer to the relevant manual.

Recommended Products

NT20, NT31 / 31C-V3, NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V4 / -AL[][]D-V4

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Controllers FAQ