Page top

Primary Contents

Question

When will the RUN output on C200HW-PA204R Power Supply Units for CS1 Programmable Controllers and C200HX/HG/HE Programmable Controllers turn ON?

Answer



The RUN output on C200HW-PA204R will turn ON when the CPU Units are in MONITOR Mode or RUN Mode as long as a fatal error has not occurred.

Normally, the RUN output turns ON approximately one second after the CPU Units power is turned ON. The RUN output will turn OFF when the CPU Units enter PROGRAM Mode or a fatal error occurs.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Controllers FAQ