![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Using CX-Programmer FA Integrated Tool Package, how can we connect Programmable Controller via Ethernet?
Answer
1. Personal Computer Ethernet setting by IP Address and Subnet Mask.
2. Ethernet Unit: IP Address, Node No., Unit No.
3. CX-Programmer and CS1 Programmable Controller is connected with Tool bus Cable.
4. CX-Programmer I/O table Window: Unit Setting (CPU bus unit System Setting) is required to be set for Ethernet [IP Address Conversion] by Automatic generation, [Sub net mask] is set.
5. CX-Programmer (CX-Net): FINS Local Routing table is created and transferred to CS1.
6. Personal Computer issues PING Command to check if Ethernet connection is OK.
7. CX-Programmer Communication Setting
1) Personal Computer Model Change / [Network Type] is set [Ethernet].
2) Click [Setting], set FINS destination address [Network] / [Node]
(Node = Ethernet Unit Node Number, Network = Network address set in Routing table)
3) Check Automatic generation method at [Driver] tab / Workstation node Address. Port Number = 9600.
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.