Page top

Primary Contents

Question

Are there comparison instructions that can be used as the input condition for other instructions in a ladder program?

Answer



In a CS/CJ-series Programmable Controllers CPU Unit, compare instructions can be used as input conditions by using Symbol Comparison Instructions.
Symbol Comparison instructions come in the three forms, LD, AND, and OR.
The AND-type symbol comparison instruction can be used with the CVM1-V2 Programmable Controllers and C200HX/HG/HE-Z Programmable Controllers CPU Unit.
The C-series Programmable Controllers CPU Units do not support Symbol Comparison Instructions.

LD (LOAD) Type (CS1/CJ1 Only)

AND (Series) Type (CS1/CJ1, C200HX/HG/HE-Z, and CVM1-V2)

OR (Parallel) Instruction (CS1/CJ1 Only)

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Controllers FAQ