Page top

Primary Contents

Question

Is it possible to connect two CPM1A Programmable Controller Units with a RS-232C cross cable through an adapter, process an input to one CPM1A Unit, and output the result from the other CPM1A Unit?

Answer



Data in the LR Area can be transferred using a CPM1A 1:1 link. Transfer the necessary data to the LR Area to use this function. DM 6650 must be set to use a 1:1 link. In this case, the baud rate will be set to 19,200 bps and cannot be changed.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Controllers FAQ