Page top

Primary Contents

Question

What is indirect DM addressing?

Answer



Indirect DM addressing involves reading the contents of a specified DM word and using it as the address of another word in the DM Area, e.g., to read the contents of the second word.

In a program, this operates as follows:

The constant 0000 is not moved to DM 0100, but rather the contents of DM 0100, which is 0500, is taken as an address in the DM Area and the constant 0000 is moved to DM 0500.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Controllers FAQ