Page top

Primary Contents

Question

Is there a cable available that will connect the built-in RS-232C port of CS-series Programmable Controllers CPU Unit to NT-AL001 Option of Programmable Controllers?

Answer



Yes, XW2Z-070T-1 (70 cm) and XW2Z-200T-1 (2 m) Cables.

These cables can also be used to connect the C200HX/HG/HE or CQM1H Programmable Controllers to the NT-AL001 RS-232C/RS-422A Link Adapter.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Controllers FAQ