Page top

Primary Contents

Question

What is the difference between C200H-ID216 Programmable Controllers’ input Units and C200H-ID218 Programmable Controllers’ input Units?

Answer



The C200H-ID216 and C200H-ID218 have different input impedances. The input impedance of each Unit follows.

C200H-ID218: 3.9 kΩ

C200H-ID216: 5.6 kΩ

Therefore, their input currents are also different.

C200H-ID218: 6 mA

C200H-ID216: 4.1 mA

Choose Units based on the leakage current of the connected devices.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Controllers FAQ