Page top

Primary Contents

Question

With the CX-Programmer FA Integrated Tool Package, what is the procedure to transfer a program to a C200HX/HG/HE-Z Programmable Controllers or C200HS Programmable Controllers Memory Cassette? What is the procedure to verify the data?

Answer



The procedure to write data to a Memory Cassette and perform verification follows.

1.Set SW1 on the Memory Cassette to OFF (write-enabled) before turning ON power supplies to the C200HX.

2.Turn ON power supplies to C200HX and then connect online.

3.Set the operating mode of the CX-Programmer to PROGRAM Mode.
Select "View" - "Window" - "Watch Window", right-click in the Watch Window, and select "Add" from the menu.
Set the address to A270.00.
Right-click the Programmable Controllers name (New Programmable Controller 1) displayed in the Watch Window, and select Set from Set/Reset in the menu.

4.To verify the data, set the address to A270.02, right click on the Programmable Controllers name (New Programmable Controller 1) displayed in the Watch Window, and select Set from Set/Reset in the menu.

5.To check the verification result, set the address to A270.03 and check the value.
The verification result is stored in A270.03 in the following manner.
1: Memory Cassette data and user memory data are different.
Or verification is not possible because CPU Unit is not in PROGRAM mode.
0: Memory Cassette data and user memory data are the same.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Controllers FAQ