![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
When using C200H-CT001-V1/CT002/CT021 High-speed Counter Units, the RUN indicator does not light even when I turn ON power supplies to Programmable Controllers. Is the Unit malfunctioning?
Answer
The RUN indicator on High-speed Counter Units lights when count operations begin. The conditions under which count operation will begin depend on the operating mode.
Example:
Using C200H-CT001-V1 in Linear Operating Mode
When bit 00 of word n allocated to the High-speed Counter Unit turns ON, the counting operation will begin, and the RUN indicator will light.
n = 100 +10 x Unit number for the C200HX/HG/HE, C200HS, or C200H
n = 2000 + 10 x Unit number for a CS1-series Programmable Controllers
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.