Page top

Primary Contents

Question

What is the advantage of using index registers?

Answer



The most beneficial use of index registers is to reduce the number of steps required in ladder programming.

When processing a continuous or uniformly spaced list of addresses in a ladder program, the exact same programming pattern may appear 10 to 20, or even hundreds of times. This can be true for sequence control (bit processing) and data processing (word processing) as well. In these situations, the number of steps used in a ladder program can be greatly reduced by using an index register in a FOR-NEXT loop.

The CVM1, CV500/CV1000/CV2000, and CS1/CJ1 Programmable Controllers' support index registers.

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Controllers FAQ