![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Is it necessary to create I/O tables when using CJ1 Programmable Controllers?
Answer
There are two ways to allocate I/O with CJ1.
Automatic I/O Allocation When Power Is Turned ON
The I/O tables will be automatically created when the power is turned ON based on the information on the Units that are actually installed in Programmable Controllers.
User Allocation
The user creates the I/O tables using Programming Devices.
If a Unit connection check (using Programming Devices to verify that the Units registered in the I/O tables are actually present) or word reservations are required, the user must create the I/O tables or the user must transfer them to the CPU Unit.
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.