Page top

Primary Contents

Question

What is the difference between C1000H/C2000H-CPU01 Programmable Controllers and C1000H/C2000H-CPU01-V1?

Answer



C1000H/C2000H-CPU01-V1 supports SYSMAC LINK.

C1000H-SLK21-V1 SYSMAC LINK Units can be used for coaxial cable, and C1000H-SLK11 can be used for fiber optic cable.

With C1000H/C2000H-CPU01-V1, up to two of the following Units can be used: Host Link Units (C500-LK203 and C500-LK103), SYSMAC NET Units (C500-SNT31-V4), and SYSMAC LINK Units (C1000H-SLK21-V1 and C1000H-SLK11).

Recommended Products

NT20,NT31/31C-V3,NT631C-V3

Better SYSMAC Compatibility and Easier-to-use Support Software

NS Series

NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.

CXONE-AL[][]C-V3 / -AL[][]D-V3

The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.

Other Programmable Controllers FAQ