![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
How do I write a program that uses index registers and increment instructions to do an incremental count of N pulse inputs?
Answer
The following introduces a method to count 32 pulse input bits within a loop program using FOR-NEXT instructions and an index register. (FOR-NEXT instructions can be used on CS1 and CJ1 Programmable Controllers (PLC).)
Key Points About This Program
Under basic operating principles, differentiated instructions and instructions with the @ option cannot be used within loop programs. Therefore the program in the following figure has been used.
Basic Structure of a Program to Generate Differentiated Bit
Program
Count input bits: CIO 0.00 to CIO 1.15 (32 bits): Processed with index register IR0
BCD, 4 digits, incremental counter: D100 to D131 (32 bits): Processed with index register IR1
Differentiated Bit Generated Flag: W0.00 to W1.15 (32 bits): Processed with index register IR2
Better SYSMAC Compatibility and Easier-to-use Support Software
NS-series PTs navigate all areas of machine operation, from daily operation to error recovery.
The CX-One is a comprehensive software package that integrates PLC Programming Software with Support Software for setting up Networks, Programmable Terminals, Servo Systems, Inverters, and Temperature Controllers.