![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country.
Please contact OMRON Europe B.V. in Netherlands.
Question
How do I program repeatedly turning a bit OFF for 1 second and ON for 1.5 seconds?
Answer
If the ON and OFF time is 0.5 s or 0.1 s, a Clock Pulse Bit (P_ls and P_0_2s) can be used as an input. The following method can be used to create a flicker program that outputs a pulse-train for ON and OFF times for which Clock Pulse Bits are not provided.
Operation Specifications and Data Trace Results
CIO 000000: Flicker start bit (CIO 0.00)
CIO 000200: Flicker bit (CIO 2.00)
*When the flicker start (CIO 0.00) turns ON, the flicker bit (CIO 2.00) is turned OFF for 1 second and ON for 1.5 s. The flicker bit will stop turning ON and OFF when the start bit turns OFF.
Ladder Programming
Programming: CS1/CJ1-series Programmable Controllers
*By changing the settings of the OFF timer (TIM 0001) and ON timer (TIM0002), the desired pulse-train output can be achieved.