Page top

Lead Contents

FAQ02296 of Safety Door Switches FAQ

FAQ No. FAQ02296

Primary Contents


What are the adjustable head directions and possible points to insert the operation key for D4DS Safety-door Switches?


As shown in the following figure, the Head can be adjusted into four directions (directions 1 to 4 in the figure) and the key can be inserted at eight points (points 1 to 8 in the figure).

Recommended Products


For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.


Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner


Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Door Switches FAQ