Page top

Lead Contents

FAQ02341 of Safety Door Switches FAQ

FAQ No. FAQ02341

Primary Contents

Question

What is slow action?

Answer



SPST-NC + SPST-NO Contact (Slow Action) Example

SPST-NC + SPST-NO contact slow action has a direct opening mechanism (forcibly opened contacts) defined under EN 60497-5-1. The NC contact side is the only side with a direct opening mechanism (forcibly opened contacts).
When contact welding occur, a plunger is pushed down to open the NC contacts and break the circuit.

DPST-NC Contact (Slow Action) Example

DPST-NC contact slow action has a direct opening mechanism (forcibly opened contacts) defined under EN60497-5-1. Both NC contact sides have a direct opening mechanism (forcibly opened contacts).

Recommended Products

F3SR-B

For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.

OS32C

Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner

D40Z

Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Door Switches FAQ