Page top

Lead Contents

FAQ02438 of Safety Door Switches FAQ

FAQ No. FAQ02438

Primary Contents


The key comes out of D4DL/D4BL Safety-door Switches with a mechanical lock if I insert the key and then turn OFF the solenoid. What causes this and how can I correct it?


Cause: The release key is in the unlock position. The lock will not engage in the unlock position.

Countermeasure: Set the release key to the lock position.

Recommended Products


For Safety Light Curtain Robust & Basic New Lineup. Understanding the Indicators at a Glance.


Compact (104.5 mm), lightweight (1.3 kg) and easy-to-install Safety Laser Scanner


Supports ISO 13849-1 (PLe/Safety Category 4). Can be used on higher risk level applications by connecting to Safety Controllers.

Other Safety Door Switches FAQ