Page top

Primary Contents

Question

What should I be aware of when connecting inputs to H7E[]-N Total/Time Counters in parallel?

Answer



Be aware of the following points when connecting the count, timer, and reset inputs in parallel. Connecting a diode to prevent the reverse flow of current is particularly important for no-voltage input model.

Example: Reset Input to H7E[]-N

No-voltage Input

Note:

1.The leakage current of the transistor used for input must be less than 1 µA.

2.The forward voltage of the diode must be as low as possible (i.e., 0.1 V maximum with an If of 20 µA) so that the voltage between terminals 3 and 4 will be the specified value of 0.5 V when the reset input is ON.

Voltage Input

Recommended Products

E5CN/E5CN-U (48 x 48 mm)

New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.

H3CR-A

Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.

H5CX

DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer

Other Counters FAQ