![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Why does the Counter not count when the input signal is input?
Answer
1. The input mode and actual input may not match.
Example:
If an encoder input is used, check whether the input mode is set to Up/Down (incrementing/decrementing) C mode.
2. If the maximum counter speed is set to low speed, the pulse may be shorter than the minimum input width, preventing the Counter from counting the input. Match the maximum counting speed to the actual input width.
3. A no-voltage signal may be input to a voltage-input model.
Replace the input device with a voltage output model, or connect an external resistor if using input from an open collector.
The following diagram shows an example using the H7AN.
*Please set the input signals to "H (High)" levels, for the open-collector in the sensor to be turned off.
New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.
Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.
DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer