Page top

Primary Contents

Question

What is "Batch counting"?

Answer




Example:

The batch counting function in the H7BR-B can be used to turn ON the batch output for the preset number of batches.

The following diagram shows an example when using a repetitive operating mode (e.g., C mode) to output a packing signal as the OUT output and pack five items in one packing case.

1. Operation Application Example

To light the indicator when 100 cases have been packed (preset value (5 units) × 100 cases), set the batch counter set value to 100 and start operation. The batch output will turn ON until the target is reached.

2. Reset Method

Turn ON the batch count reset input to reset the batch output and batch count display.

Applicable Models: H7BR-B, H7CX-A4W[], H7CX-AW[]

Recommended Products

E5CN/E5CN-U (48 x 48 mm)

New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.

H3CR-A

Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.

H5CX

DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer

Other Counters FAQ