![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is the inrush current for Counters?
Answer
Using the H7BR, which has a current of approximately 10 VA (for 240 VAC, 50 Hz), as an example, an inrush current of approximately 8 A continues for approximately 2 ms when the power is turned ON.
If the Countera's power supply is turned ON/OFF with a transistor, the inrush current may damage the transistor.
Refer to the following table of inrush currents (reference values).
The blank spaces in the table indicate inrush currents that have been omitted because they are close to the steady-state current.
The values shown in the table are approximate values and should be used for reference only.
Counters
Cam Positioners /Multi-Counters
Note: The inrush current time is measured in the wave range shown in the following figure.
New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.
Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.
DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer