Page top

Lead Contents

FAQ01841 of Power Supplies FAQ

FAQ No. FAQ01841

Primary Contents


What is life expectancy (Power Supplies)?


Typically, the Power Supplies’ service life depend on the service life of the aluminum electrolytic capacitors used in the Power Supplies. When the Power Supplies are operated under proper conditions, the expected service life can be calculated from the measured electrolytic capacitor temperature. This expected service life is known as the life expectancy.

The calculated life expectancy is not equivalent to the warranty period. The life expectancy is simply the projected service life.

The expected service life calculation assumes the following conditions:

1)Rated input voltage

2)Load rate: 50%

3)Ambient operating temperature: 40°C

4)Standard mounting position

5)Continuous 24 hr/day operation

6)Fan life not included for models equipped with a fan

Recommended Products


New Models with Indication Monitor and Simple Functions for Easy System Commissioning


High-speed, High cost performance Ionization


Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Power Supplies FAQ