Page top

Lead Contents

FAQ01843 of Power Supplies FAQ

FAQ No. FAQ01843

Primary Contents

Question

What is the maintenance forecast monitor on S8VS Switch Mode Power Supply?

Answer



As time passes, the characteristics of the electrolytic capacitor inside the Power Supply deteriorate. The maintenance forecast monitor indicates the approximate time that is left until the Power Supply will stop performing sufficiently, by calculating the deterioration of the electrolytic capacitor.

Example Using S8VS-06024A

*As a guideline, replace the Power Supply within one month when the remaining years reaches 0.0 years.

Example Using S8VS-[][][]24A (Excluding S8VS-06024A)

*As a guideline, replace the Power Supply within one month when the remaining years reaches 0.0 years.

Applicable model: S8VS-[][][]A

Model numbers with the suffix "A" are equipped with the maintenance forecast monitor.

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Power Supplies FAQ