Page top

Lead Contents

FAQ01880 of Power Supplies FAQ

FAQ No. FAQ01880

Primary Contents

Question

I measured the output voltage with a tester and it is lower than the rated voltage. Can the output voltage be adjusted?

Answer



Although there are +/- output models that cannot be adjusted, the output from most Power Supplies can be adjusted by turning the voltage output adjuster (V.ADJ).

The voltage will increase when the adjuster is turned clockwise.
The voltage will decrease when the adjuster is turned counterclockwise.

The ranges in which the voltage can be adjusted are as follows:

Voltage Adjustment Ranges (Typical Examples)

Power SuppliesVoltage adjustment range
S82J Series±10%
S82K Series
(except S82K-03012/-03024/-05024)
±10%
S82K-03012/-03024/-05024-10% to +15%

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Power Supplies FAQ