Page top

Lead Contents

FAQ01907 of Power Supplies FAQ

FAQ No. FAQ01907

Primary Contents

Question

There are Power Supplies listed with a "Class 2" UL rating. What is the "Class 2" rating?

Answer



The UL Class 2 Power Units standards apply to power supplies within a limited output current and output voltage range.

The Class 2 standard is specified in UL Standard Number UL1310. In order to receive the UL Class 2 approval, the power supplies must pass UL testing as follows:

The output current does not exceed 8 A.

The output voltage does not exceed 30 VDC.

Furthermore, a benefit of using the power supplies that have received the Class 2 approval is that the output has the same Class 2 safety level. When applying for safety standards approval for the equipment, in some cases it is not necessary to obtain safety standard approval for the connected device (load) when the device (load) is connected to the output of a power supply that has received Class 2 approval.

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Power Supplies FAQ