Page top

Lead Contents

FAQ02007 of Power Supplies FAQ

FAQ No. FAQ02007

Primary Contents

Question

What size load (as a percentage of Power Supplies' rated output capacity) can be connected to S82J or S82K Series Switch Mode Power Supply?

Answer



Generally speaking, it is possible to connect a load up to 100% of the rated output capacity (see note), but there are drawbacks. When Power Supplies are operated near their rated output capacity, inrush currents and load variations may trigger the overcurrent protection function, causing the output to stop and reducing the lifetime of Power Supplies. We recommend normal operation at about 70% to 80% of the rated capacity.

Note:There are cases when it is not possible to connect a load up to 100% of the rated capacity (for example, when the Power Supply is being used in parallel operation).

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Power Supplies FAQ