Page top

Lead Contents

FAQ02011 of Power Supplies FAQ

FAQ No. FAQ02011

Primary Contents

Question

Are there models available that support parallel operation?

Answer



The following table shows the models that support parallel connection of outputs as well as the appropriate connection methods.

ModelConnection method
S82K-10024
S8T-DCBU-02
Only connect the +V and -V outputs in parallel
S82K (100 W (- P type only)
S82J (300, 600 W)
Connect the +V and -V outputs in parallel and set the parallel operation
selection switch to PARALLEL.
S8TS (12 V, 24 V)Connect the bus line connector.
S8VM (300, 600, 1,500 W)Connect CB (CN pin 5) and CBG (CN pin 6)
(Use a maximum of 80% of the total output capacity.)

Up to two of the same model can be connected in parallel for the S82K (100 W) or S8VM (300 W, 600 W, 1,500 W), up to four of the same model can be connected in parallel for the S8TS and S8T-DCBU-02, and up to five of the same model can be connected for the S82J (300, 600 W).

The above table lists the main models for which parallel connection is possible. Refer to the datasheet for each model for details.

Attempting parallel connection for models that do not support it may result in an unbalanced load current, possibly causing the rated output current to be exceeded, so the parallel connection is not possible.

Use the same length and thickness of load connection line to ensure that the voltage drop between each Power Supply and load is the same.

Recommended Products

S8VS

New Models with Indication Monitor and Simple Functions for Easy System Commissioning

ZJ-FA20

High-speed, High cost performance Ionization

S8JX

Flexible Selection of Reliability and Ease of Operation with the S8JX. New Models with Harmonic Current Suppression for a Broader Lineup.

Other Power Supplies FAQ