Page top

Primary Contents

Question

What are Time Counters?

Answer



Time Counters measure time and display the amount of time that has been measured. They are also called total time meters or hour meters. Hours is not the only unit available, however, and time can displayed in minutes, seconds, or in some cases even days.
Time Counters are not Timers. You set a specific time with Timers and an electrical signal is output when that time has elapsed. With Time Counters on the other hand, you do not set a time. They simply total the time and display that total. If you were to define the two in terms of timers, then Timers would be Preset Timers and Timer Counters would be Total Timers. Time Counters, however, have historically been classified as Counters.

Recommended Products

E5CN/E5CN-U (48 x 48 mm)

New 48 x 48-mm Basic Temperature Controller with Enhanced Functions and Performance. Improved Indication Accuracy and Preventive Maintenance Function.

H3CR-A

Multiple Operating Modes and Multiple Time Ranges. DIN 48 x 48-mm Multifunctional Timer with Wide AC/DC Power Supply Range for Both High and Low Voltages.

H5CX

DIN 48 × 48-mm Multifunction Digital Timer/2-stage Digital Timer

Other Counters FAQ