![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Can the ZX-L measure transparent objects?
Answer
Transparent objects, which allow light to pass through, cannot be measured because Reflective Smart Sensors use a PSD and Through-beam Smart Sensors use a PD. If the transparency and required accuracy are low, it might be possible to use the ZX-L for some applications. We recommend that you conduct tests with the actual object first. If the transparency and required accuracy are high, the following Sensors can be used to measure transparent objects.
CCDs enable detecting transparent objects.
Sensing with a PSD (Not suitable for transparent objects.)
A Regular Reflective Sensor that uses a PSD cannot distinguish the light reflected from the surface because it is affected by the light reflected from the other side of the object and/or the background. For this reason, displacement of the surface cannot be accurately measured. A Diffuse Reflective Sensors cannot make measurements because the diffused light is too small.
Sensing with a CCD
A Regular Reflective Sensor with a CCD can extract the light reflected from the surface because it can distinguish between the light reflected from the surface and the light reflected from the other side. For this reason, displacement of the surface can be accurately measured without being affected by the light reflected from the other side and/or the background.
Through-beam Sensors
Z4LC-series Separate-Amplifier Parallel Beam Line Sensors
The above Sensors can detect the edge of transparent objects by using a CCD in transparent object detection mode.
| Measurement method and product | Structure | Features | Application |
| CCD, Z4LC Parallel Beam Line Sensor | ![]() One-dimension CCD Image Sensor. Pixel data can be obtained. Position information can be output. | High-precision linearity (±0.1% FS) Compact body | Determining outer diameters Detecting edge positions (including transparent objects) Determining pin pitch Detecting bar positions |
3Z4L-series Laser Micrometers
The above Micrometers can be used to detect the outer diameter or edge position of transparent objects using a laser scan method as the measurement principle.
| Measurement method and product | Structure | Features | Application |
| Laser scan, 3Z4L Laser Micrometer | ![]() Scans a narrow light beam. Measures the outer diameter by taking the time that the light is blocked as the width. | High cost High-precision linearity (±0.01% FS max.) Outer dimension is large | Determining outer diameters (including transparent objects) Detecting edge positions (including transparent objects) Determining pin pitch |
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.