![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
How many times can the zero reset be used?
Answer
The zero reset can be used up to approximately 100,000 times. This is because the default setting specifies that every time the zero reset is used, the zero reset value must be stored in internal memory. Therefore, when even when power is interrupted, the zero reset value will revert to the previous status set by the zero reset function when the power is turned ON again.
If there is no need to save the zero reset value, you can use the zero reset an unlimited number of times by going to FUN mode and setting (ZRMEN) under (SPCL) to (OFF).
Actual indications on a panel.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.