![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
How far away must surrounding objects be for them not to affect E4PA Ultra Sonic Displacement/Measuring Sensor?
Answer
For example, if the sensing distance of the E4PA-LS400-M1 is set to 1 m, the following characteristics data shows that the spread of ultrasonic waves from the center of the Sensor is approximately 250 mm. This means that if there are objects within 250 mm, they will be detected. Leave ample space surrounding the Sensor. Place any object at least 375 mm away (1.5 times the minimum distance).
E4PA-LS400-M1
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.