![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
How long does the Laser Diode (LD) last?
Answer
The LD lasts for approximately 50,000 hours at 40°C with failure rate of 10%.
It lasts for approximately 100,000 hours at normal temperature (Approx. 25°C).
The life of semiconductor laser has approx. 50,000 hours.
(Failure rate: 10%, ambient temperature: 40°C)
*Semiconductor laser is operates the pulse of one-fifth duty for keeping the long life.
*The life of Semiconductor laser becomes the approx. 50% by increasing the 10°C.
For your information, the Smart Sensors has the function of laser life degradation detection.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.