![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
How far should E4PA Ultrasonic Sensor be separated from each other?
Answer
Separate the Sensors as specified in the following table when using two or more Sensors in close proximity to one another.
Parallel Arrangement:
| Model | Y |
| E4PA-LS50-M1 | 0.3 m min. |
| E4PA-LS200-M1 | 1 m min. |
| E4PA-LS400-M1 | 2 m min. |
| E4PA-LS600-M1 | 2.5 m min. |
Note:The values shown in the table are for reference only. The actual values will vary depending on the surface conditions of the sensing object, and on the ultrasonic waves that are reflected. Moreover, if the sensing object is inclined, the Y value in the table will be increased further.
Facing Arrangement:
| Model | Y |
| E4PA-LS50-M1 | 2 m min. |
| E4PA-LS200-M1 | 8 m min. |
| E4PA-LS400-M1 | 16 m min. |
| E4PA-LS600-M1 | 25 m min. |
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.