![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
E4PA Ultrasonic Sensors will be used to detect liquid levels, but it is difficult to move E4PA up or down when installing it. Is there an easy way to set the distance?
Answer
Using E4PA with the default settings is recommended. The rated minimum distance and rated maximum distance are already set. Setup can be completed simply by setting scaling for analog values (setting desired values for analog values such as 4 to 20 mA) using Digital Panel Indicators.
The resolution, however, will be (Maximum distance - Minimum distance)/4096.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.