![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
At the maximum sensing distance of the E4PA Ultrasonic Displacement Sensor, the output should be 20 mA but only 16 mA is output. What is causing this?
Answer
Liquid surfaces are not perfectly flat, therefore perfect reflection of the waves cannot be obtained. The linear output cannot reach its maximum value.
To use the Sensor at its maximum sensing distance (e.g., when the sensing range of the E4PA-LS400-M1, is 500 to 4,000 mm, the maximum sensing distance is 4,000 mm), the sensing surface must be perfectly flat and the waves must be vertical. Keep this in mind when positioning the Sensor.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.