![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
When measuring an object through a window (slit) by using the Optical Type Displacement Sensors, how large should the window be?
Answer
When making a window frame, note the following basic points.
(1) Not intercept the Light Emitting Beam
(2) Not intercept the Light Receiving View
The above points are the essential conditions.
The above points are the essential conditions.
(3) Light should not reflect diffusely on the window frame
If the light reflecting off the object returns to the window frame and enters in the receiving area of the sensor, errors may occur.
Light returns more or less to the window frame depending on how the sensing object inclines or how the light reflects.
Whether or not this reflecting light affects the measurement depends on the amount of diffuse light, reflectance ratio of the window frame, and required measurement accuracy.
It is ideal for the window frame to be made of a material as thin as possible with matte black finish which does not reflect light.
Confirm the dimensions of the window frame, checking the measurement accuracy.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.