![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
How can the analog signal output 4-20mA of the Displacement Sensors be covered to 1-5V?
Answer
The conversion can be achieved in such a way that a voltage of 1-5V is taken from the analog output terminals to which the resistance of 250 Ω (1/4W or more) is connected in parallel.
Example:
Connection between the Displacement Sensor (analog signal output 4-20mA) and the Digital Panel Meter (DC voltage input type)
*It is required that the connecting resistance value is within the allowable load resistance of analog output of the Displacement Sensor.
*Be aware that the tolerance of resistance value of 250 Ω indicates an error of output voltage.
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.