![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
Is the setting for the number of samples to average used for the linear output?
Answer
Yes, it is. When the number of samples to average is set, the measurement values are averaged, and the value is displayed on the Amplifier Unit and sent to the linear output.
Averaging is performed using a moving average.
Applicable models: ZX-L-N Smart Sensors, ZX-E Smart Sensors, and ZX-T Series Smart Sensors
Standard Sensors for Detecting Ferrous Metals under Standard Conditions
OMRON's Fiber Sensors continue to support an increasing range of applications.
Real color sensors equipped with 2-million-pixel CCDs, the fastest in the industry. Nine different types of cameras are available.