Page top

Lead Contents

FAQ00123 of Programmable Controllers FAQ

FAQ No. FAQ00123

Primary Contents


What is the difference between files with the extension .CXT and .CXP that can be converted using the CX-Programmer FA Integrated Tool Package conversion utility?


CXT files (.CXT extension) are created when data from the older Support Software is imported into the CX-Programmer. CXT files are saved in text format, which can be easily read by the CX-Programmer and other utilities and applications.

Files that were created with the CX-Programmer are saved as CXP files (.CXP extension).
The contents of CXP and CXT files are the same, but CXP files are compressed binary files.
CXP files have a smaller file size allowing them to be easily saved on disks, and they can be processed at high speed.