Page top

Lead Contents

FAQ00923 of Programmable Controllers FAQ

FAQ No. FAQ00923

Primary Contents

Question

How do I create a program to input 2-digit BCD data from a digital switch to CIO 0.08 to CIO 0.15 and then move the data to specified DM Area words?

Answer



Assuming that CIO 0.00 to CIO 0.07 are allocated to other input bits, the following two conditions must be met to create the program.

1.Only the digital switch value from CIO 0.08 to CIO 0.15 is to be extracted from CIO 0.

2.The 8 bits extracted in the previous step must be moved to the lower 8 bits of a word so that they can be used in processing in the next program rung.

Use the MOVE DIGITS instruction (MOVD) to Meet Conditions 1 and 2 Above

The MOVE DIGITS instruction (MOVD) can be used to meet the conditions described in items 1 and 2 above.

Additional Information

What Is a Digit?

A "digit" is a single numeral. In this case, the instruction name MOVE DIGITS comes from the meaning to send a BCD value in digit (4-bit) increments.

Program

Operation

Note:For details on the MOVE DIGITS instruction (MOVD), refer to the Instructions Reference Manual for the relevant Programmable Controllers.