![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What is the muting function?
Answer
Muting Function
The muting function temporarily disables the safety function when a workpiece or conveying palette passes through the detection area of Safety Light Curtains or Safety Sensors.
F3SN/F3SL-series Safety Light Curtains and F3SH-series Multi-beam Safety Sensors do not have a muting function, but the muting function can be used if F3SP-U2P Muting Controller for Safety Sensors (sold separately) is used in conjunction with these products. Refer to the following application example.
Example Application Using the Muting Function by Combining an F3SN with an F3SP-U2P
Note:
The F3SP-U2P Muting Controller distinguishes between workpieces and people passing through by the timing of the detection by Muting Sensors A and B.
Adjust where Muting Sensors A and B are installed and the sensing direction so that the passage of a person does not interrupt the beams from both Sensors.
Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards
The updated F3SJ is even easier to use.
Operator Presence Detection in Work Areas with Complex Shapes.