![]()
Global
These are navigation links to move inside this page.
![]()
Quick links to OMRON IA in your country / territory.
Please contact our European headquarters.
Question
What are Type 2 and Type 4?
Answer
There are two types of Safety Light Curtains that are compatible with IEC 61496-1 and IEC 61496-2.
Type-2 Safety Light Curtains can be used for systems in categories B, 1, and 2. Type-4 Safety Light Curtains can be used for all categories.
Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards
The updated F3SJ is even easier to use.
Operator Presence Detection in Work Areas with Complex Shapes.