Page top

Primary Contents

Question

What is an auxiliary output?

Answer



F3SN/F3SH Series Safety Light Curtains

The default setting of the output is the reverse signal of the control output. It is only an auxiliary output, so do not use it as a control output for a safety circuit.

For F3SN-A and F3SH Series, the output operation mode can be selected using F39-MC11 Setting Console.

Dark-ON output = Control output and its reverse signal (default setting)

Light-ON output = Synchronized with the control output

Light diagnosis output

Lockout output

Outermost-beam monitoring output

Specified-beam output

Blanking monitoring output (F3SN-A only)

F3SL Series Safety Light Curtain

A signal is output in sync with the control output. It is only an auxiliary output, so do not use it as a control output for a safety circuit.

Recommended Products

D4N

Upgraded Safety Limit Switches Based on the Popular D4D, Providing a Full Lineup Conforming to International Standards

F3SJ Ver.2

The updated F3SJ is even easier to use.

OS3101

Operator Presence Detection in Work Areas with Complex Shapes.

Other Safety Sensors FAQ